|  |  | 日本語  | Português
NEW Products

 
 
 
 
Automated Inspection with Automatic Tool Changers
Creaform specializes in portable 3D measurement and analysis technologies. From handheld scanners to turnkey inspection cells, Creaform helps its customers increase quality and productivity through the design and manufacture of cutting-edge products. Fully-automated, quality control inspection solutions such as the new MetraSCAN 3D-R and CUBE-R offer users versatility, reliability, and speed without compromising accuracy. They are also entirely hands-free which increases safety.

The MetraSCAN 3D-R utilizes a patented optical scanner mounted to a robot arm for increased flexibility; it can be deployed in a new system or retrofitted to an existing application. The CUBE-R takes the automation concept even further by placing the entire inspection system in a closed cell. Both solutions provide users with an integrated approach to automated inspection and are ideal for quality assurance of automotive and aerospace components.

Inspection and verification of attributes such as shape, thickness, trim, location of holes, etc. of multiple different parts and materials is easy since the systems can be programmed offline and calibrated automatically. The MetraSCAN 3D-R and CUBE-R both include Creaform’s Autocalibration Kit which helps things keep running smoothly. Users don't have to stop the process to change from one part inspection to the next or to recalibrate the equipment.

Using ATI's QC-11 Tool Changer and Tool Stands, the Autocalibration Kit enables each system to recalibrate before moving on to the next inspection job. The master side of the ATI Tool Changer is mounted to the robot. When it's time to inspect a new part, the robot picks up the Autocalibration Kit from the tool stand by automatically coupling the master and tool sides of the Tool Changer. The robot moves the Autocalibration Kit into position and goes through a sequence to optimize scanning parameters before returning it to the tool stand. The application of ATI's automatic tool changer in the Autocalibration Kit is straightforward, but significant; it brings reliability and efficiency while saving space and increasing safety.

The MetraSCAN 3D-R and CUBE-R deliver totally automated inspection solutions that integrate multiple aspects of quality assurance verification throughout production. The systems leverage machine power and innovative programming to produce repeatable 3D analyses of parts and help manage potential quality issues further up the supply chain. The data from inspections aids in overall process improvement as well by helping to signal the appropriate times for preventive maintenance and identifying defects before they reach customers.

The safety benefits of automated systems are numerous, and can result not only in better working conditions, but also higher levels of job involvement. The MetraSCAN 3D-R and CUBE-R systems free workers from tedious inspection tasks and potential hazards by moving them into more engaging roles, such as system programming and design. Jerome-Alexandre Lavoie, Product Manager at Creaform, says that these products help to initiate a significant mindset shift in the culture of their users. “These systems encourage users to focus on ‘Quality Assurance' throughout the production process,” Lavoie says. “Instead of chasing and containing defects after they reach a customer, MetraScan 3D-R and CUBE-R users can prevent those defects from ever leaving the plant."

Of the Creaform-ATI relationship, Lavoie shares that, “Our main focus is cutting edge measurement technologies; it was clear that we needed to partner with a strong and solid robotic equipment provider such as ATI. The reliability of the ATI components has been perfect so far. We are very happy with this relationship and can’t wait for upcoming new products!”

Through innovative automation, both ATI and Creaform are changing the way work gets done. Leveraging human skill and experience with automated technology enables a higher level of production quality in manufacturing. It also helps keep people safe and engaged as it moves manufacturing technology further into the future.

For more information about Creaform's automated quality control inspections, click here.

For more information about ATI's Robotic Tool Changers, click here.

[Img1Link]


[Img2Link]
Photos courtesy of Creaform. Top - MetraScanR System, Middle - Robotic Pickup of AutoCalibration Kit, Bottom - closeup of AutoCalibration Kit with ATI Tool Changer



 
 



Compliance Devices
  
© 2026
 
 

       

Privacy Policy Novanta  • Sales Terms & Conditions  • Purchasing Terms & Conditions  • CCPA Novanta