LEARN MORE WITH ATI AND 3M'S FREE WEBINAR ON MATERIAL REMOVAL
On Thursday, May 14th, Noon-1pm (ET), ATI Industrial Automation and 3M co-presented the free webinar, "The Three Pillars of Successful Robotic Material Removal". View the recording to hear real-world examples of the benefits of robotic material removal, gain a better understanding of how to create success in this emerging field, nd discover best practices in choosing end-of-arm tooling and abrasives to best suit unique needs.


ROBOTIC SANDING MADE EASY WITH ATI’S AOV-10 AND 3M ABRASIVES
ATI Industrial Automation’s AOV-10 Axially-Compliant Orbital Sander is the ideal robotic solution for surface preparation and finishing. With built-in compliance, the AOV-10 is well-suited for many different robotic application types—even those that require a light touch. Manual material removal jobs, often labeled as dull, dirty, and dangerous, need responsiveness to ensure consistent results. ATI’s Axially-Compliant Orbital Sander provides a direct replacement for manual surface preparation and finishing techniques: high quality results without the safety hazards or compromised labor.


MESH AND ATI INNOVATE A NEW MATERIAL REMOVAL SOLUTION
MESH Automation specializes in the design and development of automated manufacturing solutions for factories. Recently, they teamed up with ATI Industrial Automation on a material removal solution for deburring small engine pistons. Their customer needed to update an outdated and underperforming finishing and inspection operation. For this automotive customer, MESH integrated the small format MINI MAC automation platform which includes a CNC machine, two robotic arms, an ATI Deburring Tool, and a gripper tool.


ATI DEVELOPS COBOT-READY ACCESSORY KITS
Cobot-Ready Accessory Kits from ATI offer users a simple and effective way to increase the flexibility of collaborative robots. ATI’s Cobot-Ready Accessory Kits are suited for a wide variety of industries and application types and include solutions for tool changing, force sensing, and material removal. Tasks such as machine tending, finishing processes, part inspection and analysis, assembly, and many other complex tasks are simple to implement with these all-in-one packages. Each kit includes the end-effector, all necessary interface plates, fasteners, connectors, cables and more to get users up and running quickly.


ATI'S F/T SENSORS HELP SURGEONS STAY IN TOUCH
A surgeon’s ability to use their knowledge and intuition to carry out procedures makes them highly efficient and sought-after experts in their respective fields. By using their experiences along with their senses, surgeons literally operate by feel and can make adjustments in real-time along the way. Teaching a robot to perform a task as complex as surgery on a human is challenging as this type of automation equipment features very limited functionality. A robot on its own has no memory or senses and offers little in the way of dynamic control or active assistance. However, with technology like ATI’s Force/Torque Sensors, robots have the ability to feel their environment.


AUTOMATED INSPECTION WITH ATI TOOL CHANGERS
Creaform specializes in portable 3D measurement and analysis technologies. From handheld scanners to turnkey inspection cells, they help customers increase quality and productivity through designing and manufacturing cutting-edge products. Fully-automated, quality control inspection solutions such as their new MetraSCAN 3D-R and CUBE-R offer users versatility, reliability, and speed without compromising accuracy. They are also entirely hands-free which increases safety. Using ATI's QC-11 Tool Changer and Tool Stands enables each system to recalibrate quickly and handle multiple jobs in one cycle.




COMPLIANT RECIPROCATING TOOL
ATI's new CRT-12-5 Compliant Reciprocating Tool is a high-precision material removal solution for robotic filing and finishing. It provides the same results as manual techniques without compromising employee safety.

PASSIVE COMPLIANT FORCE CONTROL DEVICE
The Passive Compliant Force Control (PCFC) device is used to incorporate adjustable passive compliant force control into automated material removal applications. Modular compliance force allows users to target specific force ranges for particular applications.


F/T SENSOR PRECISION ASSEMBLY DEMONSTRATION
ATI Force/Torque Sensors give robots a sense of touch by sending force and torque data to the robot. Learn how this data can be used to enable a robot to perform precision assembly tasks.

COMPLIANT DEBURRING BLADE WITH AUTOMATIC BLADE CHANGING
ATI Industrial Automation's Compliant Deburring Blade features a robust interface to attach blades and media commonly found in hand deburring tools. Pneumatically-actuated compliance allows fast and simple programming of the robot.